DICMULOBUI1.2.840.10008.5.1.4.1.1.4UI81.3.12.2.1107.5.2.30.25008.30000009112609222046800000036UI1.2.840.10008.1.2.1UI1.3.12.2.1107.5.2SHMR_VB17ACS ISO_IR 100CSORIGINAL\PRIMARY\M\ND\FM\FILDA20091126TM102242.812000 UI1.2.840.10008.5.1.4.1.1.4UI81.3.12.2.1107.5.2.30.25008.30000009112609222046800000036 DA20091126!DA20091126"DA20091126#DA200911260TM095625.359000 1TM102242.796000 2TM101910.432500 3TM102242.812000 PSH`CSMRpLOSIEMENS PNLOAvanto@SQ>bPUI1.2.840.10008.5.1.4.1.1.4UUI81.3.12.2.1107.5.2.30.25008.30000009112609222046800000037bPUI1.2.840.10008.5.1.4.1.1.4UUI81.3.12.2.1107.5.2.30.25008.30000009112609222046800000038bPUI1.2.840.10008.5.1.4.1.1.4UUI81.3.12.2.1107.5.2.30.25008.30000009112609222046800000039!STForce Anonymity PN pd_tse_cor LO Anonymous 0DA@CSO CSSHOULDER CSSE!CS SK\SP\OSP "CS#CS2D$SH tseR2d1_5 %CSN PDS3 DS2200DS23DS1 DS 63.612039 SH1HIS1 DS1.5 DS3.3 IS480 IS5 DS75DS100 DS120  LO syngo MR B17QSHBodyUS@CSROW DS180 CSN DS1.1377539270923 DS0 QCSHFS LOSIEMENS MR HEADER CS IMAGE NUM 4  LO1.0  DS209885SHFastSHNoSL SL IS0\0\0 FD;d^GR W@DS0.39DS1 IS13000 UI81.3.12.2.1107.5.2.30.25008.30000009112609222046800000034 UI81.3.12.2.1107.5.2.30.25008.30000009112609222046800000035 SH IS8 IS1 IS7 2DS2-163.97605063399\-46.739860756686\92.344516532269 7DSd0.70891902846795\0.70528987733843\3.21404597e-008\-0.0503983126238\0.05065768845969\-0.997443636846 RUI81.3.12.2.1107.5.2.30.25008.30000009112609222046800000033 @LO ADS88.903651048284 (US(CS MONOCHROME2 (US@(US@(0DS0.4375\0.4375 (US(US (US (US(US(US) (PDS831 (QDS1830(ULOAlgo1 )LOSIEMENS CSA HEADER)LOSIEMENS MEDCOM HEADER2)CS IMAGE NUM 4 ) LO20091126)OB$SV10SMEchoLinePosition hgN ISM M 240 EchoColumnPosition 1M 1M 1M ISM M 160 EchoPartitionPositiond7iISM M 8 UsedChannelMaskISEgN hgNUL M M 15 Actual3DImaPartNumberEEhgN ISICE_DimsMRC1ULEhgN hgNLOMMX_1_1_1_1_1_1_4_1_1_7_1_30B_value IS5dISFilter1LO ISFilter2ISNISProtocolSliceNumberSM MISM M 6 RealDwellTimeISnrCnISM M 13000 PixelFileISUNPixelFileNameIS.0UNSliceMeasurementDuration~DSMM209885.00000000SequenceMaskUN}vnsrtstus|~UL M M 134217737AcquisitionMatrixTextSHMM240*320MeasuredFourierLines 4 ISM M 0 FlowEncodingDirection-20 p9 } DSISFlowVencISdBdt_limittImagePixelVaFDPhaseEncodingDirectionPositiveISM M 1 NumberOfImagesInMosaic SM MUS DiffusionGradientDirectionStim_faktor 10FDImageGroupUSUS SliceNormalVector10000000000 } FDDiffusionDirectionality78 M CSTimeAfterStartFD M 0 DSM M 0.39000000FlipAngle CS M 0 DSSequenceNameDS M 0 SHRepetitionTime DS M M 2171DSEchoTimeble."">SH { 1 } { "PhoenixMetaProtocol" 1000002 2.0 { { { "false" "true" } } { 1 } { " { ""MultiStep Controller"" 1000001 666.0 { 34 400 ""Multistep Protocol"" 401 ""Step"" 402 ""Inline Composing"" 403 ""Composing Group"" 404 ""Last Step"" 405 ""Composing Function"" 406 ""Inline Combine"" 407 ""Enables you to set up a Multistep Protocol."" 408 ""Indicates the number of the current Step of the Multistep Protocol.\nPress the + button to add a Step at the end of the list.\nPress the - button to delete the current Step."" 409 ""Invokes Inline Composing."" 410 ""Identifies all Steps that will be composed."" 411 ""Defines the last measurement step of a composing function."" 412 ""Save all measurements of the Multistep Protocol into one series."" 413 ""Defines the composing algorithm to be used."" 414 ""Prio Recon"" 415 ""Enables Prio Recon measurement"" 416 ""Auto Align Spine"" 417 ""Enables the Auto Align Spine mode in GSP when protocol is open"" 422 ""Auto Coil Select"" 423 ""If set to """"Default"""",\nglobal settings from the queue menu will be used."" 424 ""On"" 425 ""Off"" 426 ""Default"" 429 ""Wait for user to start"" 430 ""Load images to graphic segments"" 431 ""Before measurement"" 432 ""After measurement"" 433 ""1st segment"" 434 ""2nd segment"" 435 ""3rd segment"" 436 ""All segments"" 445 ""Angio"" 446 ""Spine"" 447 ""Adaptive"" } { { } { { ""false"" ""true"" } } { { { } { } { } { } } { { } { } { } { } } } { {