DICMULOBUI1.2.840.10008.5.1.4.1.1.4UI61.3.12.2.1107.5.2.30.277.30000009071006005807800000317UI1.2.840.10008.1.2.1UI1.3.12.2.1107.5.2SHMR_VB17ACS ISO_IR 100CSORIGINAL\PRIMARY\M\DIS2DDA20090701TM142652.609000 UI1.2.840.10008.5.1.4.1.1.4UI61.3.12.2.1107.5.2.30.277.30000009071006005807800000317 DA20090701!DA20090701"DA20090701#DA200907010TM135535.531000 1TM142652.593000 2TM142403.205000 3TM142652.609000 PSH`CSMRpLOSIEMENS PNLOVerio @SQ8`PUI1.2.840.10008.5.1.4.1.1.4UUI61.3.12.2.1107.5.2.30.277.30000009071006005807800000318`PUI1.2.840.10008.5.1.4.1.1.4UUI61.3.12.2.1107.5.2.30.277.30000009071006005807800000319`PUI1.2.840.10008.5.1.4.1.1.4UUI61.3.12.2.1107.5.2.30.277.30000009071006005807800000320!STForce Anonymity PNpd_tse_fs_tra_p2_fov_110 LO Anonymous 0DA@CSO  CSSE!CS SK\SP\OSP "CSSAT1\FS #CS2D$SH tseR2d1_7 %CSN PDS3 DS5630DS30DS1 DS 123.177027SH1HIS1 DS3 DS3.3 IS383 IS7 DS80DS100 DS100  LO syngo MR B17QSHBodyUS@CSCOL DS133 CSN DS1.9307304101838 DS0 QCSFFS LOSIEMENS MR HEADER CS IMAGE NUM 4  LO1.0  DS164002.5SHFastSHNoSL SL IS0\0\0 FD߁4@|JXRlĽ4DS1.13DS1 IS15600 UI61.3.12.2.1107.5.2.30.277.30000009071006005807800000315 UI61.3.12.2.1107.5.2.30.277.30000009071006005807800000316 SH IS9 IS1 IS21 2DS020.507321511645\-74.567903350849\-20.74127843669 7DSf0.99920051699679\0.00348722263579\0.03982670098863\-2.83235744e-008\0.99618859440334\-0.0872254801116 RUI61.3.12.2.1107.5.2.30.277.30000009071006005807800000314 @LO ADS-27.964590834816(US(CS MONOCHROME2 (US@(US@(0DS0.34375\0.34375 (US(US (US (US(US(US(PDS438 (QDS840 (ULOWINDOW1 )LOSIEMENS CSA HEADER)LOSIEMENS MEDCOM HEADER2)CS IMAGE NUM 4 ) LO20090701)OB\%SV10SMEchoLinePositionoH =)nISM M 192 EchoColumnPosition5F ISM M 160 EchoPartitionPositionrH ISM M 8 UsedChannelMask5FLtH UL M M 255 Actual3DImaPartNumber=)nISICE_Dims=)nvH LOMMX_1_1_1_1_1_1_8_1_1_21_1_188B_value=)n5FwH wH ISFilter1=)n5FyH (yH (yH ISFilter2=)n5FlzH lzH ISProtocolSliceNumber=)nISM M 14 RealDwellTime=)nISM M 15600 PixelFile=)n5FUNPixelFileName5FH UNSliceMeasurementDurationlH DSMM164002.50000000SequenceMaskH =)npH UL M M 134217728AcquisitionMatrixTextH H SHMM256*320MeasuredFourierLines=)nH H ISM M 0 FlowEncodingDirectionF::lstarteDSOriginalSeriesNumberCsaBaseImage::myISOriginalImageNumberogISImaAbsTablePositionL*ISLM M 0 M 0 M -1296 NonPlanarImageCsaBaseImageUS M M 1 MoCoQMeasure:myImagePixel.PObject::__whatyvUS LQAlgorithmObject::__whatvSHSlicePosition_PCS%L3FDM M 20.50732151 M -74.56790335 M -20.74127844RBMoCoTrans5<FDRBMoCoRotDCsaBaseImage::mySyngoPrivateExteFDMultistepIndexe::mySeries.PObject::__whatrISM M 0 ImaRelTablePositionL<ISM M 0 M 0 M 0 ImaCoilString;L> LOMMC:FARFSWDDataType2L@SHM M predictedGSWDDataTypeProperties.Sound.PrNW y9 perties.Sound.PoSHM M predictedNormalizeManipulatedLoad.InlinePositionDisplay"" ""Properties.AISImaPATModeTextLOMMp2B_matrixFDBandwidthPerPixelPhaseEncodeFDFMRIStimulLevelA[`\FKDH8+A+^ZmFDMosaicRefAcqTimeswmry\I?7OJ;?,.6/.*~y}tqu}FDAutoInlineImageFilterEnabled"Ue[zBbggs||~ISM M 1 QCDatayexvqtt{hs|jEC^U{i_NbFD)CSMR)LO20090701) OBx0SV10AMUsedPatientWeightPObject::__whatISM M 65 NumberOfPrescanscsDLISM M 0 TransmitterCalibrationDSM M 379.73947000PhaseGradientAmplitudeCsaPersFound::myUserInfofDSM M 0.00000000ReadoutGradientAmplitudee|DSM M 0.00000000SelectionGradientAmplitude'LDSM M 0.00000000GradientDelayTimeer1LDSM M 18.00000000 M 16.00000000 M 16.00000000RfWatchdogMaskto4LISM M 0 RfPowerErrorIndicatoraS7LDSSarWholeBodyDi2L DSSedyBLDSMM1000000.00000000M1784.78493071M1784.67665888SequenceFileOwnerS=SHMMSIEMENSStim_mon_mode.CsaUPString::unistrISM M 2 Operation_mode_flagions.CsaCUAttrStrings::datanISM M 0 dBdt_maxibration.CsaAttrStrings::data.CsaVList::mycdata.CDSM M 0.00000000t_puls_maxnLDSM M 0.00000000dBdt_threshOfLastCalibration.CsaAttrStrings::data.CsaVList { "PhoenixMetaProtocol" 1000002 2.0 { { { "false" "true" } } { 1 } { " { ""MultiStep Controller"" 1000001 666.0 { 34 400 ""Multistep Protocol"" 401 ""Step"" 402 ""Inline Composing"" 403 ""Composing Group"" 404 ""Last Step"" 405 ""Composing Function"" 406 ""Inline Combine"" 407 ""Enables you to set up a Multistep Protocol."" 408 ""Indicates the number of the current Step of the Multistep Protocol.\nPress the + button to add a Step at the end of the list.\nPress the - button to delete the current Step."" 409 ""Invokes Inline Composing."" 410 ""Identifies all Steps that will be composed."" 411 ""Defines the last measurement step of a composing function."" 412 ""Save all measurements of the Multistep Protocol into one series."" 413 ""Defines the composing algorithm to be used."" 414 ""Prio Recon"" 415 ""Enables Prio Recon measurement"" 416 ""Auto Align Spine"" 417 ""Enables the Auto Align Spine mode in GSP when protocol is open"" 422 ""Auto Coil Select"" 423 ""If set to """"Default"""",\nglobal settings from the queue menu will be used."" 424 ""On"" 425 ""Off"" 426 ""Default"" 429 ""Wait for user to start"" 430 ""Load images to graphic segments"" 431 ""Before measurement"" 432 ""After measurement"" 433 ""1st segment"" 434 ""2nd segment"" 435 ""3rd segment"" 436 ""All segments"" 445 ""Angio"" 446 ""Spine"" 447 ""Adaptive"" } { { } { { ""false"" ""true"" } } { { { } { } { } { } } { { } { } { } { } } } { {