DICMULOBUI1.2.840.10008.5.1.4.1.1.4UI81.3.12.2.1107.5.2.30.25008.30000009102611091292100000017UI1.2.840.10008.1.2.1UI1.3.12.2.1107.5.2SHMR_VB17ACS ISO_IR 100CS ORIGINAL\PRIMARY\M\DIS2D\FM\FIL DA20090929TM221350.796000 UI1.2.840.10008.5.1.4.1.1.4UI81.3.12.2.1107.5.2.30.25008.30000009102611091292100000017 DA20090929!DA20090929"DA20090929#DA200909290TM215422.109000 1TM221350.703000 2TM221121.407500 3TM221350.796000 @SSALOIMA NONEPSH`CSMRpLOSIEMENS PNLOAvanto@SQbPUI1.2.840.10008.5.1.4.1.1.4UUI81.3.12.2.1107.5.2.30.25008.30000009102611091292100000018bPUI1.2.840.10008.5.1.4.1.1.4UUI81.3.12.2.1107.5.2.30.25008.30000009102611091292100000019!STForce Anonymity LOSPI RELEASE 1 LO001SNYDC062009093002540235PN pd_tse_cor LO Anonymous 0DA@CSO LOSPI RELEASE 1 LOERROR  CSSE!CS SK\SP\OSP "CS#CS2D$SH *tse2d1_9 %CSN PDS2 DS3000DS33DS1 DS 63.670397 SH1HIS1 DS1.5 DS2.2 IS450 IS9 DS70DS100 DS170  LO syngo MR B15QSHBodyUS@CSCOL DS120 CSN DS1.1782172865543 DS0 QCSFFS LOSIEMENS MR HEADER CS IMAGE NUM 4  LO1.0  DS147680SHNormalSHNoSL qSL pIS0\0\1 FDIN]UR(6QfxI@DS2.225 DS1 IS9100 UI81.3.12.2.1107.5.2.30.25008.30000009102611091292100000015 UI81.3.12.2.1107.5.2.30.25008.30000009102611091292100000016 SH IS6 IS1 IS12 2DS2-119.13938935079\-22.159923992703\52.433361855392 7DSd0.8928184683307\0.43406175831235\0.12027290874676\0.17778420818641\-0.0942639581597\-0.9795443234033 RUI81.3.12.2.1107.5.2.30.25008.30000009102611091292100000014 @LO ADS20.992294016451 (US(CS MONOCHROME2 (US@(US@(0DS 0.375\0.375 (US(US (US (US(PDS801 (QDS1658(RDS0 (SDS1 (TLOUS(ULOWINDOW1 )LOSIEMENS CSA HEADER)LOSIEMENS MEDCOM HEADER2)CS IMAGE NUM 4 ) LO20090929)OB<$SV10RMEchoLinePositiona4f9a0acb4e8fb23eb6fa3555cea08f6d39c71ded2e3e17ISM M 225 EchoColumnPositionSliceNo"> { } 0.DSM M 0.00000000ReadoutGradientAmplitude1500><DSM M 0.00000000SelectionGradientAmplitudex@` ` 8y@` ` DSM M 0.00000000GradientDelayTimex@` ` 8y@` ` DSM M 13.00000000 M 13.00000000 M 10.00000000RfWatchdogMask x@@` @` 8y@X` X` ISM M 0 RfPowerErrorIndicator.000` ` } ` ` DSSarWholeBody8K } DSSedyParag"> 1_1_DSMM1000000.00000000M1384.67597903M1384.63790957SequenceFileOwner> ize> SHMMSIEMENSStim_mon_mode* { -+> 16.ISM M 2 Operation_mode_flag } ;96578<ISM M 0 dBdt_max DSM M 0.00000000t_puls_maxDSM M 0.00000000dBdt_thresh$"%#DSM M 0.00000000dBdt_limitLimi20rue"31DSM M 0.00000000SW_korr_faktor 1>i  ;ogPMDSM M 1.00000000Stim_max_online { 448 } { "PhoenixMetaProtocol" 1000002 2.0 { { { "false" "true" } } { 1 } { " { ""MultiStep Controller"" 1000001 666.0 { 33 400 ""Multistep Protocol"" 401 ""Step"" 402 ""Inline Composing"" 403 ""Composing Group"" 404 ""Last Step"" 405 ""Composing Function"" 406 ""Inline Combine"" 407 ""Enables you to set up a Multistep Protocol."" 408 ""Indicates the number of the current Step of the Multistep Protocol.\nPress the + button to add a Step at the end of the list.\nPress the - button to delete the current Step."" 409 ""Invokes Inline Composing."" 410 ""Identifies all Steps that will be composed."" 411 ""Defines the last measurement step of a composing function."" 412 ""Save all measurements of the Multistep Protocol into one series."" 413 ""Defines the composing algorithm to be used."" 414 ""Prio Recon"" 415 ""Enables Prio Recon measurement"" 416 ""Auto Align Spine"" 417 ""Enables the Auto Align Spine mode in GSP when protocol is open"" 422 ""Auto Coil Select"" 423 ""If set to """"Default"""",\nglobal settings from the queue menu will be used."" 424 ""On"" 425 ""Off"" 426 ""Default"" 429 ""Wait for user to start"" 430 ""Load images to graphic segments"" 431 ""Before measurement"" 432 ""After measurement"" 433 ""1st segment"" 434 ""2nd segment"" 435 ""3rd segment"" 436 ""All segments"" 445 ""Angio"" 446 ""Spine"" } { { } { { ""false"" ""true"" } } { { { } { } { } { } } { { } { } { } { } } } { {