DICMUL¶OBUI1.2.840.10008.5.1.4.1.1.4UI81.3.12.2.1107.5.2.30.25008.30000009102611091292100000030UI1.2.840.10008.1.2.1UI1.3.12.2.1107.5.2SHMR_VB17ACS ISO_IR 100CSORIGINAL\PRIMARY\M\DIS2DDA20090929TM222423.234000 UI1.2.840.10008.5.1.4.1.1.4UI81.3.12.2.1107.5.2.30.25008.30000009102611091292100000030 DA20090929!DA20090929"DA20090929#DA200909290TM215422.109000 1TM222423.046000 2TM222047.585000 3TM222423.234000 @SSALOIMA NONEPSH`CSMRpLOSIEMENS PNLOAvanto@SQ>þÿàbPUI1.2.840.10008.5.1.4.1.1.4UUI81.3.12.2.1107.5.2.30.25008.30000009102611091292100000031þÿàbPUI1.2.840.10008.5.1.4.1.1.4UUI81.3.12.2.1107.5.2.30.25008.30000009102611091292100000032þÿàbPUI1.2.840.10008.5.1.4.1.1.4UUI81.3.12.2.1107.5.2.30.25008.30000009102611091292100000033!STForce Anonymity LOSPI RELEASE 1 LO001SNYDC062009093002542809PNpd_tse_fs_tra  LO Anonymous 0DA@CSO LOSPI RELEASE 1 LOERROR  CSSE!CS SK\SP\OSP "CSSAT2\SFS#CS2D$SH *tseR2d1_8%CSN PDS3 €DS3390DS45ƒDS1 „DS 63.670322 …SH1H†IS1 ‡DS1.5 ˆDS3.3 ‰IS512 ‘IS8 “DS100 ”DS100 •DS180  LO syngo MR B15QSHBodyUSCSROW DS180 CSN DS2.0500853077735 DS0 QCSFFS LOSIEMENS MR HEADER CS IMAGE NUM 4  LO1.0  DS214490SHFastSHNoSL qûÿÿSL nûÿÿIS0\0\3 FDµ£YU:SÀ—æÀYTVÀÝ¡›Üséø?DS2.8125DS1 IS10800 UI81.3.12.2.1107.5.2.30.25008.30000009102611091292100000028 UI81.3.12.2.1107.5.2.30.25008.30000009102611091292100000029 SH IS9 IS1 IS8 2DS2-76.906636559527\-89.317978122001\4.5569952633479 7DSd0.8549797678495\0.45125552215996\0.25569131836682\-0.4488743872024\0.89076097175267\-0.0711103066783 RUI81.3.12.2.1107.5.2.30.25008.30000009102611091292100000027 @LO ADS29.198648951848 (US(CS MONOCHROME2 (US(US(0DS0.46875\0.46875 (US(US (US (US(PDS230 (QDS571 (RDS0 (SDS1 (TLOUS(ULOAlgo1 )LOSIEMENS CSA HEADER)LOSIEMENS MEDCOM HEADER2)CS IMAGE NUM 4 ) LO20090929)OB¨$SV10RMEchoLinePositiona4f9a0acb4e8fb23eb6fa3555cea08f6d39c71ded2e3e17ISM M 256 ÍÍÍÍÍEchoColumnPositionSliceNo"> { } 0.ÿÿÿÿDSM M 0.00000000ÍÍÍÍÍReadoutGradientAmplitudeÿÿÿÿ1500><ÿÿÿÿDSM M 0.00000000ÍÍÍÍÍSelectionGradientAmplitudeèx@ ¦`  ¦` 8y@¸¦` ¸¦` DSM M 0.00000000ÍÍÍÍÍGradientDelayTime˜x@ð§` ð§` 8y@¨` ¨` DSM M 13.00000000 M 13.00000000 M 10.00000000ÍÍÍRfWatchdogMask èx@@©` @©` 8y@X©` X©` ISM M 0 ÍÍÍÍÍRfPowerErrorIndicator.000ª` ª` } ¨ª` ¨ª` DSÍSarWholeBodyÿÿÿÿà8Kþÿÿÿÿÿÿÿ } DSÍSedyParaÿÿÿÿg"> ÿÿÿÿ1_1_DSMM1000000.00000000M2170.16569847M2170.16569847ÍÍÍSequenceFileOwnerÿÿÿÿ> ÿÿÿÿize> SHMMSIEMENSÍÍÍÍÍStim_mon_mode*ÿÿÿÿ { -+ÿÿÿÿ> 16.ISM M 2 ÍÍÍÍÍOperation_mode_flagÿÿÿÿ } ;9ÿÿÿÿ6578<ISM M 0 ÍÍÍÍÍdBdt_maxÿÿÿÿÿÿÿ ÿÿÿÿDSM M 0.00000000ÍÍÍÍÍt_puls_maxÿÿÿÿÿÿÿÿÿDSM M 0.00000000ÍÍÍÍÍdBdt_thresh$"ÿÿÿÿ%#ÿÿÿÿDSM M 0.00000000ÍÍÍÍÍdBdt_limitÿLimi20ÿÿÿÿrue"31ÿÿÿÿDSM M 0.00000000ÍÍÍÍÍSW_korr_faktor 1ÿÿÿÿ>i àê Ùý ;ÃogPMì°DSM M 1.00000000ÍÍÍÍÍStim_max_online { 448 } { "PhoenixMetaProtocol" 1000002 2.0 { { { "false" "true" } } { 1 } { " { ""MultiStep Controller"" 1000001 666.0 { 33 400 ""Multistep Protocol"" 401 ""Step"" 402 ""Inline Composing"" 403 ""Composing Group"" 404 ""Last Step"" 405 ""Composing Function"" 406 ""Inline Combine"" 407 ""Enables you to set up a Multistep Protocol."" 408 ""Indicates the number of the current Step of the Multistep Protocol.\nPress the + button to add a Step at the end of the list.\nPress the - button to delete the current Step."" 409 ""Invokes Inline Composing."" 410 ""Identifies all Steps that will be composed."" 411 ""Defines the last measurement step of a composing function."" 412 ""Save all measurements of the Multistep Protocol into one series."" 413 ""Defines the composing algorithm to be used."" 414 ""Prio Recon"" 415 ""Enables Prio Recon measurement"" 416 ""Auto Align Spine"" 417 ""Enables the Auto Align Spine mode in GSP when protocol is open"" 422 ""Auto Coil Select"" 423 ""If set to """"Default"""",\nglobal settings from the queue menu will be used."" 424 ""On"" 425 ""Off"" 426 ""Default"" 429 ""Wait for user to start"" 430 ""Load images to graphic segments"" 431 ""Before measurement"" 432 ""After measurement"" 433 ""1st segment"" 434 ""2nd segment"" 435 ""3rd segment"" 436 ""All segments"" 445 ""Angio"" 446 ""Spine"" } { { } { { ""false"" ""true"" } } { { { } { } { } { } } { { } { } { } { } } } { {