DICMULOBUI1.2.840.10008.5.1.4.1.1.4UI61.3.12.2.1107.5.2.30.277.30000009071006005807800000542UI1.2.840.10008.1.2.1UI1.3.12.2.1107.5.2SHMR_VB17ACS ISO_IR 100CSORIGINAL\PRIMARY\M\ND DA20090709TM131539.578000 UI1.2.840.10008.5.1.4.1.1.4UI61.3.12.2.1107.5.2.30.277.30000009071006005807800000542 DA20090709!DA20090709"DA20090709#DA200907090TM125952.765000 1TM131539.515000 2TM131306.402500 3TM131539.578000 PSH`CSMRpLOSIEMENS PNLOAvanto@SQ8`PUI1.2.840.10008.5.1.4.1.1.4UUI61.3.12.2.1107.5.2.30.277.30000009071006005807800000543`PUI1.2.840.10008.5.1.4.1.1.4UUI61.3.12.2.1107.5.2.30.277.30000009071006005807800000544`PUI1.2.840.10008.5.1.4.1.1.4UUI61.3.12.2.1107.5.2.30.277.30000009071006005807800000545!STForce Anonymity PNpd_tse_fs_tra  LO Anonymous 0DA@CSO CSKNEE CSSE!CS SK\SP\OSP "CSSAT1\FS #CS2D$SH tse2d1_15 %CSN PDS3 DS5210DS47DS1 DS 63.612449 SH1HIS1 DS1.5 DS3.3 IS450 IS15DS85DS100 DS182  LO syngo MR B17QSHTxRx_15Ch_KneeUS@CSROW DS150 CSN DS0.10825587959079DS0 QCSFFS LOSIEMENS MR HEADER CS IMAGE NUM 4  LO1.0  DS151830SHFastSHNoSL SL IS0\0\0 FD۞fҘ{NR'xF@DS4.185 DS1 IS8600 UI61.3.12.2.1107.5.2.30.277.30000009071006005807800000540 UI61.3.12.2.1107.5.2.30.277.30000009071006005807800000541 SH IS3 IS1 IS12 2DS2-183.83613532367\-73.231352712383\45.284938812256 7DSF0.87714616458681\-0.4802234958336\0\0.4802234958336\0.87714616458681\0 RUI61.3.12.2.1107.5.2.30.277.30000009071006005807800000539 @LO ADS45.284938812256 (US(CS MONOCHROME2 (US@(US@(0DS0.4375\0.4375 (US(US (US (US(US(US(PDS407 (QDS768 (ULOWINDOW1 )LOSIEMENS CSA HEADER)LOSIEMENS MEDCOM HEADER2)CS IMAGE NUM 4 ) LO20090709)OB$SV10SMEchoLinePositionPObject::__whatISM M 225 EchoColumnPositioncMgeLISM M 160 EchoPartitionPositionISM M 8 UsedChannelMaskCsaPersFound::myUserInfofUL M M 32767 Actual3DImaPartNumberalue|TISICE_Dims'LLOMMX_1_1_1_1_1_1_25_1_1_12_1_13B_valueL *ISFilter10CsaBaseViewing::myVoiLUTISFilter2CsaBaseViewing::myExplanation.CsaCUPString::sortISProtocolSliceNumber_LISM M 18 RealDwellTimeISM M 8600 PixelFileUNPixelFileNameUNSliceMeasurementDurationDSMM151830.00000000SequenceMaskUL M M 134217736AcquisitionMatrixTextSHM M 272*320sMeasuredFourierLinesISM M 0 FlowEncodingDirectionISFlowVencFDPhaseEncodingDirectionPositiveISM M 1 NumberOfImagesInMosaicUS DiffusionGradientDirectionFDImageGroupUS SliceNormalVectorFDDiffusionDirectionalityCSTimeAfterStartDSM M 4.18500000FlipAngleDSSequenceNameSHRepetitionTimeDSEchoTimeDSNumberOfAveragesDSVoxelThicknessDSVoxelPhaseFOVDSVoxelReadoutFOVDSVoxelPositionSagDSVoxelPositionCorDSVoxelPositionTraDSVoxelNormalSagDSVoxelNormalCorDSVoxelNormalTraDSVoxelInPlaneRotDSImagePositionPatientDSImageOrientationPatientDSPixelSpacingDSSliceLocationDSSliceThicknessDSSpectrumTextRegionLabelSHComp_AlgorithmISComp_BlendedISComp_ManualAdjustedISComp_AutoParamLTComp_AdjustedParamLTComp_JobIDLTFMRIStimulInfoISFlowEncodingDirectionStringSHRepetitionTimeEffectiveDSCsiImagePositionPatientDSCsiImageOrientationPatientDSCsiPixelSpacingDSCsiSliceLocationDSCsiSliceThicknessDSOriginalSeriesNumberISOriginalImageNumberISImaAbsTablePositionSLM M 0 M 0 M -1400 NonPlanarImageUS M M 0 MoCoQMeasureUS LQAlgorithmSHSlicePosition_PCSFDMM-183.83613532 M -73.23135271 M 45.28493881RBMoCoTransFDRBMoCoRotFDMultistepIndexISM M 0 ImaRelTablePositionISM M 0 M 0 M 0 ImaCoilStringLOMMC:K15RFSWDDataTypeSHM M predictedGSWDDataTypeSHM M predictedNormalizeManipulatedISImaPATModeTextLOB_matrixFDBandwidthPerPixelPhaseEncodeFDFMRIStimulLevelFDMosaicRefAcqTimesFDAutoInlineImageFilterEnabledISM M 1 QCDataFD)CSMR)LO20090709) OB&SV10AMUsedPatientWeightISM M 65 NumberOfPrescansISM M 0 TransmitterCalibrationDSM M 68.69357900PhaseGradientAmplitudeDSM M 0.00000000ReadoutGradientAmplitudeDSM M 0.00000000SelectionGradientAmplitudeDSM M 0.00000000GradientDelayTimeDSM M 12.00000000 M 13.00000000 M 9.00000000RfWatchdogMaskISM M 0 RfPowerErrorIndicatorDSSarWholeBodyDSSedyDSMM1000000.00000000 M 18.36031910 M 18.35268210SequenceFileOwnerSHMMSIEMENSStim_mon_modeISM M 2 Operation_mode_flagISM M 0 dBdt_maxDSM M 0.00000000t_puls_maxDSM M 0.00000000dBdt_threshDSM M 0.00000000dBdt_limitDSM M 0.00000000SW_korr_faktorDSM M 1.00000000Stim_max_onlineDSM M 3.41725183 M 12.81713867 M 12.46024132Stim_max_ges_norm_onlineDSM M 0.60837144Stim_limDSM M 45.73709869 M 27.64929962 M 31.94370079Stim_faktorDSM M 1.00000000CoilForGradientSHMMvoidCoilForGradient2SHMMAS05CoilTuningReflectionDSCoilIdIS M M 255 M 92 M 238 M 238 M 108 M 238 M 238 M 177 M 238 M 178 M 238 MiscSequenceParam&IS*M M 0 M 0 M 0 M 0 M 0 M 0 M 0 M 0 M 0 M 0 M 0 M 0 M 0 M 0 M 0 M 0 M 0 M 0 M 0 M 0 M 0 M 0 M 0 M 0 M 32 M 0 M 0 M 0 M 0 M 0 M 0 M 6326 M 0 M 0 M 0 M 0 M 0 M 0 MrProtocolVersionISM M 21710006DataFileNameLORepresentativeImageUIPositivePCSDirectionsSHMM+LPHRelTablePositionISM M 0 M 0 M 0 ReadoutOSFDM M 2.00000000LongModelNameLOM M NUMARIS/4SliceArrayConcatenationsISM M 1 SliceResolutionDSM M 1.00000000AbsTablePositionISM M -1400 AutoAlignMatrixFLMeasurementIndexFLCoilStringLOMMC:K15PATModeTextLOPatReinPatternSTM##M#1;FFS;65.00;60.00;2;0;0;-483458107ProtocolChangeHistoryUS M M 0 IsocenteredUS M M 0 MrPhoenixProtocolUNM M { "PhoenixMetaProtocol" 1000002 2.0 { { { "false" "true" } } { 1 } { " { ""MultiStep Controller"" 1000001 666.0 { 34 400 ""Multistep Protocol"" 401 ""Step"" 402 ""Inline Composing"" 403 ""Composing Group"" 404 ""Last Step"" 405 ""Composing Function"" 406 ""Inline Combine"" 407 ""Enables you to set up a Multistep Protocol."" 408 ""Indicates the number of the current Step of the Multistep Protocol.\nPress the + button to add a Step at the end of the list.\nPress the - button to delete the current Step."" 409 ""Invokes Inline Composing."" 410 ""Identifies all Steps that will be composed."" 411 ""Defines the last measurement step of a composing function."" 412 ""Save all measurements of the Multistep Protocol into one series."" 413 ""Defines the composing algorithm to be used."" 414 ""Prio Recon"" 415 ""Enables Prio Recon measurement"" 416 ""Auto Align Spine"" 417 ""Enables the Auto Align Spine mode in GSP when protocol is open"" 422 ""Auto Coil Select"" 423 ""If set to """"Default"""",\nglobal settings from the queue menu will be used."" 424 ""On"" 425 ""Off"" 426 ""Default"" 429 ""Wait for user to start"" 430 ""Load images to graphic segments"" 431 ""Before measurement"" 432 ""After measurement"" 433 ""1st segment"" 434 ""2nd segment"" 435 ""3rd segment"" 436 ""All segments"" 445 ""Angio"" 446 ""Spine"" 447 ""Adaptive"" } { { } { { ""false"" ""true"" } } { { { } { } { } { } } { { } { } { } { } } } { {