DICMULOBUI1.2.840.10008.5.1.4.1.1.4UI61.3.12.2.1107.5.2.30.277.30000009071006005807800000289UI1.2.840.10008.1.2.1UI1.3.12.2.1107.5.2SHMR_VB17ACS ISO_IR 100CS$ORIGINAL\PRIMARY\M\NORM\DIS2D\FM\FILDA20090701TM141055.531000 UI1.2.840.10008.5.1.4.1.1.4UI61.3.12.2.1107.5.2.30.277.30000009071006005807800000289 DA20090701!DA20090701"DA20090701#DA200907010TM135535.531000 1TM141055.484000 2TM140816.840000 3TM141055.531000 PSH`CSMRpLOSIEMENS PNLOVerio @SQ8`PUI1.2.840.10008.5.1.4.1.1.4UUI61.3.12.2.1107.5.2.30.277.30000009071006005807800000290`PUI1.2.840.10008.5.1.4.1.1.4UUI61.3.12.2.1107.5.2.30.277.30000009071006005807800000291`PUI1.2.840.10008.5.1.4.1.1.4UUI61.3.12.2.1107.5.2.30.277.30000009071006005807800000292!STForce Anonymity PNpd_tse_cor_p2  LO Anonymous 0DA@CSO  CSSE!CS SK\SP\OSP "CSPFP\SAT1#CS2D$SH tseR2d1_9 %CSN PDS3 DS4500DS52DS1 DS 123.177036SH1HIS1 DS3 DS3.3 IS507 IS9 DS75DS100 DS257  LO syngo MR B17QSHBodyUSCSROW DS150 CSN DS1.3716819475952 DS0 QCSFFS LOSIEMENS MR HEADER CS IMAGE NUM 4  LO1.0  DS149190SHFastSHNoSL SL IS0\0\0 FDBw@RFCPx=@DS1.0325DS1 IS3800 UI61.3.12.2.1107.5.2.30.277.30000009071006005807800000287 UI61.3.12.2.1107.5.2.30.277.30000009071006005807800000288 SH IS5 IS1 IS17 2DS05.9008450135621\-39.007393710704\29.698068165645 7DSd0.97234996808614\0.23352845557423\2.1731355e-009\0.01342954267157\-0.0559170109975\-0.9983450982825 RUI61.3.12.2.1107.5.2.30.277.30000009071006005807800000286 @LO ADS-40.949653580907(US(CS MONOCHROME2 (US(US(0DS0.2734375\0.2734375 (US(US (US (US(US(USC(PDS766 (QDS1492(ULOWINDOW1 )LOSIEMENS CSA HEADER)LOSIEMENS MEDCOM HEADER2)CS IMAGE NUM 4 ) LO20090701)OB$SV10SMEchoLinePositionEvL``LvLISM M 288 EchoColumnPositionEvL``LvLISM M 256 EchoPartitionPositionEvL``ISM M 8 UsedChannelMaskEvLUL M M 255 Actual3DImaPartNumberEvLISICE_DimsEvLLOMMX_1_1_1_1_1_1_9_1_1_17_1_169B_valueSLvLol> EvLISFilter1LvLr"" EvLISFilter2LvL""InEvLISProtocolSliceNumberEvLISM M 16 RealDwellTimevLoil EvLISM M 3800 PixelFileLvL""2nEvLUNPixelFileNamevL EvLUNSliceMeasurementDurationEvLDSMM149190.00000000SequenceMaskLvL } EvLUL M M 134217728AcquisitionMatrixTextEvLSHM M 384p*512MeasuredFourierLinesEvLISM M 0 FlowEncodingDirectionEvLISFlowVencLvLion.EvLFDPhaseEncodingDirectionPositiveEvLISM M 1 NumberOfImagesInMosaicEvLUS DiffusionGradientDirectionEvLFDImageGroupLvL> { EvLUS SliceNormalVector00EvLFDDiffusionDirectionalityEvLCSTimeAfterStartL EvLDSNumberOfAverages"">EvLDSVoxelThicknessLe.""EvLDSVoxelPhaseFOVvLbel>EvLDSVoxelReadoutFOV EvLDSVoxelInPlaneRot EvLDSImagePositionPatientEvLDSImageOrientationPatientEvLDSPixelSpacingLvL.""IEvLDSSliceLocationvL.IsLEvLDSSliceThicknessLy"">EvLDSSpectrumTextRegionLabelEvLSHComp_AlgorithmLep""EvLISComp_BlendedLvLencyEvLISComp_ManualAdjustedEvLISComp_AutoParamL ::mycdata.CsaPListBase::ldISM M -1296 AutoAlignMatrix4FLMeasurementIndexdata.CsaPListBase::iteratorpFLCoilStringleSetID.CsaUPString::unistrLOMMC:FAPATModeTextdyComponentStatusIDLOMMp2PatReinPatternPCsaSeries::mySpecificCharactSTM##M#1;FFS;65.00;22.00;1;0;0;1053946837ProtocolChangeHistory:lstartQUS M M 0 Isocentered\CsaSeries::mySeriesHidden.DbUS M M 0 MrPhoenixProtocolsition_flag.CsaFlag::myValuexUNMM { "PhoenixMetaProtocol" 1000002 2.0 { { { "false" "true" } } { 1 } { " { ""MultiStep Controller"" 1000001 666.0 { 34 400 ""Multistep Protocol"" 401 ""Step"" 402 ""Inline Composing"" 403 ""Composing Group"" 404 ""Last Step"" 405 ""Composing Function"" 406 ""Inline Combine"" 407 ""Enables you to set up a Multistep Protocol."" 408 ""Indicates the number of the current Step of the Multistep Protocol.\nPress the + button to add a Step at the end of the list.\nPress the - button to delete the current Step."" 409 ""Invokes Inline Composing."" 410 ""Identifies all Steps that will be composed."" 411 ""Defines the last measurement step of a composing function."" 412 ""Save all measurements of the Multistep Protocol into one series."" 413 ""Defines the composing algorithm to be used."" 414 ""Prio Recon"" 415 ""Enables Prio Recon measurement"" 416 ""Auto Align Spine"" 417 ""Enables the Auto Align Spine mode in GSP when protocol is open"" 422 ""Auto Coil Select"" 423 ""If set to """"Default"""",\nglobal settings from the queue menu will be used."" 424 ""On"" 425 ""Off"" 426 ""Default"" 429 ""Wait for user to start"" 430 ""Load images to graphic segments"" 431 ""Before measurement"" 432 ""After measurement"" 433 ""1st segment"" 434 ""2nd segment"" 435 ""3rd segment"" 436 ""All segments"" 445 ""Angio"" 446 ""Spine"" 447 ""Adaptive"" } { { } { { ""false"" ""true"" } } { { { } { } { } { } } { { } { } { } { } } } { {