DICMULOBUI1.2.840.10008.5.1.4.1.1.4UI61.3.12.2.1107.5.2.30.277.30000009071406015231200000087UI1.2.840.10008.1.2.1UI1.3.12.2.1107.5.2SHMR_VB17ACS ISO_IR 100CSORIGINAL\PRIMARY\M\NORM\DIS2D DA20090714TM103623.937000 UI1.2.840.10008.5.1.4.1.1.4UI61.3.12.2.1107.5.2.30.277.30000009071406015231200000087 DA20090714!DA20090714"DA20090714#DA200907140TM100428.781000 1TM103623.093000 2TM103031.242500 3TM103623.937000 PSH`CSMRpLOSIEMENS PNLOVerio @SQ8`PUI1.2.840.10008.5.1.4.1.1.4UUI61.3.12.2.1107.5.2.30.277.30000009071406015231200000088`PUI1.2.840.10008.5.1.4.1.1.4UUI61.3.12.2.1107.5.2.30.277.30000009071406015231200000089`PUI1.2.840.10008.5.1.4.1.1.4UUI61.3.12.2.1107.5.2.30.277.30000009071406015231200000090!STForce Anonymity PN pd_tse_sag LO Anonymous 0DA@CSO  CSSE!CS SK\SP\OSP "CS#CS2D$SH tseR2d1_4 %CSN PDS2.5 DS2600DS23DS1 DS 123.176965SH1HIS1 DS3 DS2.75IS544 IS4 DS100 DS100 DS180  LO syngo MR B17QSHBodyUS@@CSROW DS150 CSN DS1.4508768525218 DS0 QCSHFS LOSIEMENS MR HEADER CS IMAGE NUM 4  LO1.0  DS352445SHFastSHNoSL SL IS0\0\-33 FD. G@W GԮtK@DS1.88DS1 IS8700 UI61.3.12.2.1107.5.2.30.277.30000009071406015231200000085 UI61.3.12.2.1107.5.2.30.277.30000009071406015231200000086 SH IS10 IS1 IS12 2DS047.997562472581\-46.084337234497\22.914581833417 7DS*0\1\0\0.64278762731871\0\-0.7660444283238 RUI61.3.12.2.1107.5.2.30.277.30000009071406015231200000084 @LO ADS51.497474992948 (US(CS MONOCHROME2 (US@(US@(0DS0.46875\0.46875 (US(US (US (US(US(US (PDS1130(QDS2182(ULOAlgo1 )LOSIEMENS CSA HEADER)LOSIEMENS MEDCOM HEADER2)CS IMAGE NUM 4 ) LO20090714)OB$SV10SMEchoLinePositionp ct::__w=)nISM M 272 EchoColumnPosition5F sDLISM M 160 EchoPartitionPositions  ISM M 8 UsedChannelMask5F4u UL M M 3 Actual3DImaPartNumberdata.CsaVList::mycdata.CsaP=)nISICE_DimsL' =)nw LOMMX_1_1_1_1_1_1_19_1_1_12_1_35B_value=)n5Fx x ISFilter1=)n5Ftz z z ISFilter2=)n5FT{ T{ { ISProtocolSliceNumber} } =)nISM M 11 RealDwellTime~ =)n84G=)nISM M 8700 PixelFile=)n5F UNPixelFileName5F UNSliceMeasurementDurationT DSMM352445.00000000SequenceMask =)nX UL M M 134217736AcquisitionMatrixText SHMM320*320MeasuredFourierLines=)n ISM M 0 FlowEncodingDirectionF$ $ ISFlowVenc=)nh h FDPhaseEncodingDirectionPositive=)nISM M 1 NumberOfImagesInMosaic=)nUS DiffusionGradientDirectionn5FFDImageGroupn5F$ US SliceNormalVector5Ft ( FDDiffusionDirectionalityl l CSTimeAfterStart DSM M 1.88000000FlipAngle DSSequenceNameEchoColumnPositionhgNhgNSHRepetitionTimeDSEchoTimeICE_DimsDSNumberOfAveragesISDSVoxelThicknessmeDSVoxelPhaseFOVSliceMeasurementDurationDSVoxelReadoutFOVDSVoxelPositionSag M 0 DSVoxelPositionCorISM M 1 DSVoxelPositionTraUS DSVoxelNormalSagDSVoxelNormalCorDSVoxelNormalTratFOVDSVoxelInPlaneRotagDSImagePositionPatiententDSImageOrientationPatientDSPixelSpacingalAdjustedDSSliceLocationInfoDSSliceThicknessentationPatientDSSpectrumTextRegionLabelSHComp_AlgorithmNonPlanarImaISComp_BlendedSHISComp_ManualAdjustedFDRBMoCoRotISComp_AutoParamISLTComp_AdjustedParamRFSWDDataTypLTComp_JobIDdictedLTFMRIStimulInfoBandwidthPerPixelPhaseEncodeISFlowEncodingDirectionString 1 SHRepetitionTimeEffectiveDSCsiImagePositionPatientDSCsiImageOrientationPatientDSCsiPixelSpacingDSCsiSliceLocationDSCsiSliceThicknessDSOriginalSeriesNumberISOriginalImageNumberISImaAbsTablePositionSLM M 0 M 0 M -1832 NonPlanarImageUS M M 1 MoCoQMeasureUS LQAlgorithmSHSlicePosition_PCSFDM M 47.99756247 M -46.08433723 M 55.91458183RBMoCoTransFDRBMoCoRotFDMultistepIndexISM M 0 ImaRelTablePositionISM M 0 M 0 M -33 ImaCoilStringLOMMC:BO1,2RFSWDDataTypeSHM M predictedGSWDDataTypeSHM M predictedNormalizeManipulatedISImaPATModeTextLOB_matrixFDBandwidthPerPixelPhaseEncodeFDFMRIStimulLevelFDMosaicRefAcqTimesFDAutoInlineImageFilterEnabledISM M 1 QCDataFD)CSMR)LO20090714) OBSV10AMUsedPatientWeight!"&#$'#!&&++0Qe_jon oi<0((Y!*%'/&$'')%@?ISM M 65 NumberOfPrescansityz~ [95;6110///-7,KNFNBHBJ2:()432/26@51/ISM M 0 TransmitterCalibrationN:07$&3>8,53471363641,47/t69643442;6778DSM M 422.89042200PhaseGradientAmplitude654:5<@4334:8;5:656>425474Sp fE>@A@aDSM M 0.00000000ReadoutGradientAmplitudeQ374671B3 awx@DB@?8@D@?@F@983:9DSM M 0.00000000SelectionGradientAmplitudesNH`[WEYKeB@>?>;:D?;5:;<>=?gUcoC;;ODSM M 0.00000000GradientDelayTimeGFFVSAGDJBC>@>DBFH>FDOlqvW<2=?FAA@>=A:8CDSM M 18.00000000 M 16.00000000 M 16.00000000RfWatchdogMaskED?C?BA/yQ<\P-SzuZN9SEDBD=C??;>;<9e ISM M 0 RfPowerErrorIndicatorKEDHQY@CDGF:9@8Ly °¹oQUa]DSSarWholeBodyLCJDM?>A"WkrXByDSM M 0.00000000dBdt_limit< Ny]pDzJ'DSM M 0.00000000SW_korr_faktorq(]VT{U4Q[^e, DSM M 1.00000000Stim_max_onlineATv%TzII0*DSM M 10.50798416 M 10.36481953 M 3.72738409Stim_max_ges_norm_online-ZVjR}OtWl$DSM M 0.53699410Stim_limwJC>S6='*)H8/;DSM M 39.99589920 M 23.36529922 M 23.68700027Stim_faktorE_0z7}soKDSM M 1.00000000CoilForGradient=p|(!M+hb}SHMMvoidCoilForGradient21 P hH SHMMAS097CoilTuningReflectionMeasurementDuration"> { { { 272&IS*M M 0 M 0 M 0 M 0 M 0 M 0 M 0 M 0 M 0 M 0 M 0 M 0 M 0 M 0 M 0 M 0 M 0 M 0 M 0 M 0 M 0 M 0 M 0 M 0 M 32 M 0 M 0 M 0 M 0 M 0 M 0 M 375 M 0 M 0 M 0 M 0 M 0 M 0 MrProtocolVersion } { LORepresentativeImage } SHMM+LPHRelTablePosition3238300 } } 1 3 { 1 3 FLMeasurementIndex } { 320 } @AE da#C=1&*)+301425.QUHJOSTM##M#1;HFS;65.00;25.00;1;0;0;-598172970ProtocolChangeHistory v4%31/2214&;XaO__Bf6P=I10-51*175/<:2US M M 0 Isocentered=:1@:6()/ $$)79;6;5857,ic5555599G< { "PhoenixMetaProtocol" 1000002 2.0 { { { "false" "true" } } { 1 } { " { ""MultiStep Controller"" 1000001 666.0 { 34 400 ""Multistep Protocol"" 401 ""Step"" 402 ""Inline Composing"" 403 ""Composing Group"" 404 ""Last Step"" 405 ""Composing Function"" 406 ""Inline Combine"" 407 ""Enables you to set up a Multistep Protocol."" 408 ""Indicates the number of the current Step of the Multistep Protocol.\nPress the + button to add a Step at the end of the list.\nPress the - button to delete the current Step."" 409 ""Invokes Inline Composing."" 410 ""Identifies all Steps that will be composed."" 411 ""Defines the last measurement step of a composing function."" 412 ""Save all measurements of the Multistep Protocol into one series."" 413 ""Defines the composing algorithm to be used."" 414 ""Prio Recon"" 415 ""Enables Prio Recon measurement"" 416 ""Auto Align Spine"" 417 ""Enables the Auto Align Spine mode in GSP when protocol is open"" 422 ""Auto Coil Select"" 423 ""If set to """"Default"""",\nglobal settings from the queue menu will be used."" 424 ""On"" 425 ""Off"" 426 ""Default"" 429 ""Wait for user to start"" 430 ""Load images to graphic segments"" 431 ""Before measurement"" 432 ""After measurement"" 433 ""1st segment"" 434 ""2nd segment"" 435 ""3rd segment"" 436 ""All segments"" 445 ""Angio"" 446 ""Spine"" 447 ""Adaptive"" } { { } { { ""false"" ""true"" } } { { { } { } { } { } } { { } { } { } { } } } { {