With minimal accurate dose and fewer retakes, FAST CARE allows care providers to treat even the most delicate patients with the lowest radiation dose possible. See how St. Louis Children’s is reducing dose with FAST CARE.
FAST CARE works with Siemens SOMATOM Definition scanners to create an improved scanning experience for patients and technologists alike. FAST CARE automation allows for a more accurate scan. And the lowest radiation dose possible. With FAST CARE, technologists will spend less time at the scanner and more time with the patient.
Learn more about FAST CARE and how it can benefit your patients
View a video from the Perelman School of Medicine at the University of Pennsylvania and read about their investigators’ recent study from the March 26, 2012 New England Journal of Medicine titled 'CT Angiography for Safe Discharge of Patients with Possible Acute Coronary Syndromes”
In a hectic ER every second counts. See how Tacoma General is utilizing FAST CARE.
How to Save Time and Reduce Stress in Trauma CT Imaging
Download Now[717 KB]
Every patient’s situation is unique. And until now, each patient’s scan required time-consuming and complex adjustments to ensure a reliable outcome. As a consequence, a technologist’s time could be consumed at the scanner instead of with the patient.
By dramatically streamlining the CT workflow, FAST assists in every step of the examination. From planning and scanning, to image reconstruction. In some cases, FAST reduces time-consuming and complex procedures to just a click. FAST not only streamlines the workflow, but also increases the consistency of the CT images. Patients will appreciate fewer retakes because FAST helps get the results right the first time.
Exposure to radiation is always a concern for healthcare providers and patients. Therefore the principle “As Low as Reasonably Achievable” (ALARA) was central to the research and development of CARE. CARE exposes patients to the lowest radiation dose possible by providing a CT scan personalized to fit their individual needs.
CARE delivers excellent image quality with minimal radiation dose. For each patient a topogram determines the optimal acquisition parameters (kV, mA, etc.), while taking into account the goal of the study. The result is a truly personalized imaging procedure.
Learn more about FAST CARE and how it can benefit your patients
Together with syngo.via and automated setup, for example, CAREKv, Fast Spine and others, FAST CARE streamlines the complete examination, from scan preparation to data evaluation. FAST CARE ensures highly-reliable and efficient diagnosis with minimal patient burden.
With minimal accurate dose and fewer retakes, FAST CARE allows care providers to treat even the most delicate patients with the lowest radiation dose possible.
FAST CARE eliminates the “one size fits all” CT scan. It makes each scan even more personalized to the patient while reducing the number of adjustments the technologist needs to make.
Saturday, March 24 - March 27, 2012
Chicago, IL
http://accscientificsession.cardiosource.org/ACC12.aspx
Saturday, April 21 - 26, 2012
New York Hilton, New York, New York
Details TBA
http://www.asnr.org/2012/
Sunday, June 17 - 20, 2012
Hyatt Regency, San Francisco, CA
Details TBA
http://www.isct.org/mdct.html
Thursday, July 19 - 22, 2012
Marriott Baltimore Waterfront, Baltimore, Maryland
Details TBA
http://www.scct.org/annualmeeting/2012/index.cfm
Sunday, August 12 -15, 2012
Gaylord Palms, Orlando, FL
Details TBA
http://www.ahraonline.org/AM/Template.cfm?Section=AHRA2012_Orlando
September, 2012
Details TBA
http://www.erad.org/
Sunday, November 25 - November 30, 2012
McCormick Place, Chicago, IL
http://rsna2012.rsna.org/
Learn more about the key features of FAST CARE that make CT scanning more efficient and accurate.
Learn more about the key features of FAST CARE that produce a CT scan at the lowest possible dose.
Learn more about the key features of FAST CARE that allow for a greater flexibility when working with CT scans and patients.
General Demo
FAST CARE Online Demos
Learn more about FAST CARE through Online Demos.
View Demos