The Guide brings you up-to-date on what is new and developing in the field of diagnostic imaging.
Siemens has always believed that even the farthest technical horizons were temporary and could be surpassed with consistent dedication to improved healthcare. This visionary approach has made Siemens the undisputed innovation leader in CT over the past 35 years. Our innovative philosophy is based solidly upon the assumption that achieving the highest technical performance is only important when it meets the needs of the patient and our customers. From the very beginning, one of the most frequent demands of our end users has been patient safety. And in Computed Tomography, patient safety translates primarily into dose reduction.
For this reason, we have, from the earliest days, developed many significant products and protocols that follow the “As Low as Reasonably Achievable” (ALARA) principle to reduce radiation dose to the lowest possible level. This desire for as little radiation exposure as possible lies at the heart of our CARE (Combined Applications to Reduce Exposure) research and development philosophy. Over the years, Siemens has been highly successful in integrating many innovations into the Siemens scanners that significantly reduce radiation dose in comparison to other systems available on the CT market.
For example, Siemens eliminates pre- and post spiral over-radiation with the Adaptive Dose Shield introduced in 2007. This saves up to 25% dose in addition to all other dose savings.
The SOMATOM Definition Flash launched in 2008 is another prime example. Its core innovation – the revolutionary Flash Spiral – reduces dose to unprecedented levels. Consider how ground-breaking it is to acquire, for example, the whole heart in the blink-of-an-eye with less than 1 mSv.
Another benchmark for low dose CT was introduced at this year’s RSNA. With Iterative Reconstruction in Image Space (IRIS), the Siemens SOMATOM Definition scanners routinely achieve up to 60% additional dose reduction in a wide range of CT applications while maintaining excellent image quality.
A final proof of Siemens CT’s undisputed low-dose leadership comes from our customers. For the first time in CT history, Siemens encourages users to participate in the International Image Contest and share their best, low-radiation images acquired while utilizing all available low-dose solutions.
Results may vary. Data on file.
The Adaptive Dose Shield - available on the SOMATOM Definition AS and SOMATOM Definition Flash - eliminates over-radiation pre- and post-spiral to the patient (marked in red). It is unique to the CT industry and part of the innovative new STRATON X-ray tube design. By dynamically moving shields into place on the X-ray tube it blocks unnecessary dose. The Adaptive Dose Shield dynamically opens at the beginning of a spiral range and then dynamically closes at the end. Now all clinically irrelevant dose is eliminated. Not only for dedicated applications, but for every single spiral acquisition. Giving you the ability to save an additional 25% of dose in routine exams like abdominal CT.
Results may vary. Data on file.
With the introduction of the SOMATOM Definition Flash in 2008, we took on CT’s most pressing challenge and made dose reduction the centerpiece of our research. Its core innovation – the revolutionary Flash Spiral – can be summarized in four words: Flash speed. Lowest dose.
The new SOMATOM Definition Flash was therefore designed specially to make CT exams much healthier for your patients.
Flash Speed
The SOMATOM Definition Flash opens a door to new levels of patient friendliness with the speed to cover the entire thorax in less than a second – if necessary even without a breath hold. A whole body scan requires less than 5 seconds, while for perfusion or dynamic vascular imaging, long range scans become routine and gated chest CTs become sub-second procedures. Your patients will be off the table faster than ever before and can go back with positive feelings about their scan experience. Now, even demanding patients, i.e. obese and trauma patients, restless children, etc. will hardly cause a ripple in your daily routine. All can be scanned quickly and efficiently.
Lowest Dose
Maybe even more important – and impressive – is the incredible reduction in dose for all scans, resulting, e.g. in dose down to sub-mSv for cardiac imaging. In its second generation, Dual Energy automatically provides a second contrast for the best possible diagnosis without extra dose. At the same time, X-CARE allows protecting individual organs and the most radiation-sensitive body regions – for example, female breasts – by accurately and efficiently minimizing exposure.
www.siemens.com/somatom-definition-flash
Results may vary. Data on file.
Because at Siemens dose reduction has continued to be given top priority, assuring both patients and medical personnel the best in medical care with the least possible risk, we can now introduce another low dose solution – once again Siemens has set the benchmark on low dose imaging with the introduction of iterative reconstruction. With IRIS the Siemens high-end SOMATOM Definition scanners deliver excellent diagnostic image quality with levels of dose lower than ever before. With IRIS, Siemens’ smart approach to iterative reconstruction, up to 60% additional dose reduction can be achieved in a wide range of daily routine CT applications.
Dose reduction with CT has been limited by the currently used filtered back projection reconstruction algorithm as displayed on the left. When using this conventional reconstruction of acquired raw data into image data, a trade-off between spatial resolution and image noise has to be considered. Higher spatial resolution increases the ability to see the smallest detail; however, it is directly correlated with increased image noise.
In an iterative reconstruction, a correction loop is introduced into the image generation process as shown on the right. To avoid long reconstruction times the new Iterative Reconstruction in Image Space first applies a raw data reconstruction only once. During this initial raw data reconstruction, a so-called and newly developed master volume is generated that contains the full amount of raw data information, but at the expense of significant image noise. During the following iterative corrections the image noise is removed without degrading image sharpness. The new technique results in increased image quality or dose savings of up to 60 % for a wide range of clinical applications.
Iterative Reconstruction in Image Space Brochure
Results may vary. Data on file.
In a continual commitment to patient care and radiation reduction in computed tomography (CT), Siemens Healthcare
has launched SIERRA (Siemens Radiation Reduction Alliance) and has established an expert panel to advance the
cause of dose reduction in CT. The new Low Dose Expert Panel includes 15 specialists in radiology, cardiology and
physics, who are internationally recognized for their publications on the subject of CT dose. The panel’s
objective is to generate proposals for how manufacturers may continue to develop their technology and to help
users better adapt their procedures in order to bring about further dose reduction in CT. One of the most
important suggestions from the first meeting of the Low Dose Expert Panel in May concerns methods to increase
utilization in clinical practice of the many CT dose reduction technologies that are already available.
SIERRA’s expert panel proposes its first recommendations on patient care, radiation reduction
“Our aim as a leading innovator in the field of computed tomography is to reduce radiation exposure for all
typical CT examinations below 2 mSv, which is as low as the average annual dose due to naturally occurring
background radiation. We are committed to doing everything we can to help our customers reduce doses in CT
without compromising the diagnostic quality of the examination in any way,” said Sami Atiya, PhD, CEO,
Computed Tomography, Siemens Healthcare. “With this in mind, we want to work with experts to develop
concrete proposals on dose reduction and, therefore, launched Siemens Radiation Reduction Alliance,
SIERRA.”
Excellent image quality is vital in CT, but it is also important to keep the patient’s radiation exposure
as low as possible. Siemens Healthcare has already introduced a wide range of measures to help its customers
consistently achieve this goal. Now, Siemens wants to take on a more active role in this field and has convened a
panel of experts expressly to develop new ideas for dose reduction in CT.
The Low Dose Expert Panel will meet twice a year to discuss new ideas and investigate whether measures already
agreed upon are having a positive impact. Siemens intends to use the discussions to spur the development of new
features for its CT scanners and new training programs for its customers.
The panel’s members are:
Hatem Alkadhi, MD, University Hospital Zürich, Switzerland
Christoph Becker, MD, Ludwig Maximilian University, Germany
Elliot Fishman, MD, Johns Hopkins University, U.S.
Donald Frush, MD, Duke University, U.S.
Jörg Hausleiter, MD, German Heart Center Munich, Germany
Willi Kalender, PhD, University of Erlangen, Germany
Harold Litt, MD-PhD, University of Pennsylvania, U.S.
Cynthia McCollough, PhD, Mayo Clinic, U.S.
Alec Megibow, MD, NYU-Langone Medical Center, U.S.
Michael Recht, MD, NYU-Langone Medical Center, U.S.
Dushyant Sahani, MD, Harvard Medical School, Massachusetts General Hospital, U.S.
U. Joseph Schoepf, MD, Medical University of South Carolina, U.S.
Marilyn Siegel, MD, Mallinckrodt Institute of Radiology, U.S.
Aaron Sodickson, MD-PhD, Brigham and Women’s Hospital, U.S.
Kheng-Thye Ho, MD, Tan Tock Seng Hospital, Singapore
U. Joseph Schoepf, MD, Medical University of South Carolina, Charleston, U.S.
"Radiation dose from medical imaging has historically received much greater attention in Europe than in other parts of the world, where radiation exposure only recently has become a topic of discussion. On that background, Siemens has several decades of experience in the implementation of radiation reduction strategies and has a longstanding, successful track record of providing their customers with tools that deliver optimal image quality at the lowest possible radiation dose. Most of the technical features and mechanisms for radiation reduction which regulatory bodies currently consider making mandatory in the U.S. have been part of their standard portfolio and implemented in their products for many years. I am happy and proud to embark on this initiative together with Siemens and my colleagues from around the globe in order to ensure that these powerful tools are used to their fullest extent. With this endeavor we can make a difference and show to the world that we do get the message, that we can indeed change, and slash radiation dose without sacrificing diagnostic quality."
Cynthia McCollough, PhD, Mayo Clinic, Rochester, Minn, U.S.
“I see users operating CT scanners in everyday applications without taking full advantage of the possibilities available to them to strike the optimal balance between image quality and radiation dose. The answer, in my opinion, involves a significant amount of training across a wide range of areas. I want to see users at more and more institutions receive the advanced training they need in order to make best use of the options available, and this will be the main objective of my work on the panel.”
Marilyn Siegel, MD, Mallinckrodt Institute of Radiology, St. Louis, U.S.
"We have made great advances in optimizing pediatric radiation doses, but dose reduction optimization remains a work in progress. Advances in technology and capabilities of CT scanners will continue to evolve and improve our ability to diagnose disease. These advances will mandate new scanning protocols and continuing education for users. By collaborating with industry, we can optimize CT scanning in children even further and continue to improve patient care. I am delighted to join Siemens in an initiative to develop protocols and integrate new technologies into clinical practice."